Hi Ti,
I saw figure 29. internal frame sync in 960 datasheet.
this figure shows 4 input ser-camera to des IC.
I wonder :
q1) when I use internal frame sync in 960 des, is it possible below use-case ?
- 1st and 2nd input of des follows internal frame sync
- and 3rd, 4th input of des follows external frame sync (or 'using input-gpio of des, and send it to 3rd, 4th ser' GPIO output)
q2) for different image resolution and hz, (1.2M@30hz *2ea + 2M@30hz *2ea + 1.5M@60hz *2ea)
how can I make frame-sync system ? is there any, practical example for this ?
thanks