Part Number: SN65HVS882
what is spi clk supported by this device and what is DC in below figure??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVS882
what is spi clk supported by this device and what is DC in below figure??
Hi Harsh,
The SPI clock has to meet the minimums shown in the timing requirements for the system.
Below are the figures explaining the timing parameters:
There needs to be a minimum of 2 ns of recovery time, t_rec between the time LD hits 50% of its maximum value during its rise time to when the clock pulse reaches 50% of this figure. See Figure 4 for more explanation. LD is similar to the Chip Select line in SPI.
The minimum clock width, t_w1 shown in figure 5, is 4 ns.
The clock pulse frequency, f_clk, needs to be in the range 0Hz - 100MHz, the 0Hz is represented by the value "DC". This is shown in figure 5.
The clock must also conform the serial input data: the setup time, t_su1, is the minimum time between when the serial input data hits 50% of its maximum value, either rising or falling, and when the clock hits its 50% value on its rising edge, this is shown in figure 6.
The clock must also hold for a minimum of 2 ns for the input data to be registered as valid, t_H1 shown in figure 6.
Finally there is another setup time, t_su2, is the minimum time between /CE when it hits its 50% value on the falling edge and when the clock hits its 50% value on the rising edge.
If the SPI clock you are using can conform to these specifications than it will be okay to use in the application.
Best,
Parker Dodson