This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: 948 fpdlink datarate

Part Number: DS90UB948-Q1

DATASHEET 948 VERSION:REVISED NOVEMBER 2018

PAGE 23:

The DS90UB948-Q1 supports clocks in the range of 25 MHz to 96 MHz over 1 lane, or 50 MHz to 192 MHz over
2 lanes. The FPD-Link III serial stream rate is 3.36 Gbps maximum (875 Mbps minimum) or 2.975 Gbps
maximum per lane (875 Mbps minimum), respectively.

QUESTION:

Why fpd-link serial stream rate is 2.975 Gbps maximum per lane? it can works with 192Mhz clocks,why the rate could not to be with 3.36Gbps per lane?

ths!