Part Number: DS90UB935-Q1
Hi team,
There the question arose whether it is possible to use a CLK speed of the CSI-2 interface of 500MHz (1000Mbps) with a DS90UB935 module if you only use 2 CSI-2 lanes.
Then the transfer rate on the FPD link is ||| Page raw 2 Gbps and 2.5 Gbps after encoding. That is well below the maximum transfer rate of raw 2.5 Gbps and 3 Gbps after encoding.
Please support
Thanks!