Part Number: TUSB4041I
Other Parts Discussed in Thread: TPS2052C
Hi,
I would like to design a 10 port USB hub with TUSB4041I with 2 tiers. I have some design questions below to be answered.
At TIER1 there is a TUSB4041I and I will connect its downstream ports to TIER2 (2xTUSB4041I, 1xTUSB4020BI and 1xMCU via FTDI Serial Converter chip)
- Can I use same clock crystal for TIER1 and TIER2 hubs (3xTUSB4041I and 1xTUSB4020BI) or every hub should have different clock crystals?
- I am planning to use self powered hub configuration for TIER2, can I use bus powered for TIER1 and TIER2 Upstream ports or connect to 5VDC in my design?
- Should I use OVERCURxz pins for TIER1 hub? What if I have left as unconnected?
- Should I take any ESD, EMI protection measures for TIER2 to USB connectors? I think these measures are taken in TUSB4041I, but if you have any suggestion to improve these measures with extra circuit please advice.
- I would like to sense OVERCURxz pins for TIER2 with MCU for error reporting. Therefore MCU and Power Switch (TPS2052C) will be connected together. Most probably I will use an isolation circuit to isolate MCU. Do you have any connection measure advice?
Thanks for your support.