Part Number: TPS65988
Other Parts Discussed in Thread: TPD6S300
Hi,
I've trying to support the following sequence and not able to do with all Samsung phones?
The detailed description and HUB schematic are enclosed.
The PD communication messages for the Samsung phone are enclosed also.
- The phone is connected to HUB J1 connector PD Port 1 (VBUS1)
- The Charger is connected to HUB J2 connector PD Port 2 (VBUS2)
- Manually send SWSr (Swap to Source=PR_Swap) command to PD Port 1 / PR_Swap to the phone
- The phone is switched to Sink and start Charging
POC advance Port conf_Samsubg issue.pptPR_Swap Samsung S20+.xlsx