Part Number: TPS65988
Hi team,
Customer has several questions about TPS65988/7D.
please support following questions.
Q1.PP3 and PP4 equal to PP_EXT1 and 2?
Q1.1 what can VBUS Mapping configure? could you give some example?
Q2.what is the differences of following configuration? could you give some example?
Table 3-12. 0x28 Port Configuration Register Bytes1-2:Bits 5:3
000b Standard USB2-only USB-C receptacle.
001b Standard fully-featured USB-C receptacle.
010b Tethered USB2-only cable with USB-C plug.
011b Tethered fully-featured cable USB-C plug.
Q3. are there any kind of firmware installed on TPS65988/7D when shipped?
- and if yes, is it possible to customize it when shipped?
Q4. about following board.
a) TIDA_50012
b) TIDA_50014
c) TPS65988DH_Standard_v6_1_1
Only TIDA-50012 has PWM configuration register
(Table 3-93.) 0x6B HW Control Register
Can other b),c) board configure HW control register ? how?
best regards,
Takuya