This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: HSD bit rate of 947 and 948

Part Number: DS90UB947-Q1

Hi team,

customer use 4pin HSD connect 947 and 948, the transform signal is (1920x1200) and 1080p60 Resolutions with 24-Bit Color Depth

could you help on below questions:

1. What's the maxmum bit rate of each HSD cable?

2. Could you share the datasheet of HSD cable you receommended or parameter requirement?

thanks.

  • Hello Betty,

    1) Using the 947 you can trasmit:
    Over single link a data rate of 3.36Gbps
    Over dual link a data rate of 2.975Gbps/link

    2) There are many STQ cables in the market, for example : G&G122239, G&G122519, Leoni Dacar 535, Leoni Dacar 566, Leoni Dacar 636, JAE MX-48, Molex USCAR ... etc