Other Parts Discussed in Thread: ESD122, ESDS312
Hi team,
My costumer would like to know our solution for EClamp10012PQ (30V/3A) , does TI have the compatible one or similar function device for it?
Please refer to attachment. Thanks.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex
Thanks for bringing this up. At this time we don’t have a device that provides the same function as the EClamp10012PQ which looks like a 30V Termination and ESD protection device. If there isn’t a need of the termination and just ESD with lower voltage like 3.6V, the ESDS312 or ESD122 is a very good option but doesn’t match the features of the EClamp10012PQ
Thanks and let me know if you have any follow up
Regards
Obi Oji