Part Number: DS90UB935-Q1
Other Parts Discussed in Thread: ALP, USB2ANY
Hello, I've designed system utilising DS90UB935-Q1 and DS90UB936 deserializer. PoC is built with reference parts. Due to size challenges on the serialiser side coax (RG-316) is directly soldered to PCB. On the receiver side we are using SMA. Transmission line was evaluated with VNA (twice: in our lab and in external laboratory specialised with RF measurement). There were no issues found (operating margins are probably safe).
Serialiser is receiving single data pair MIPI CSI-2 signal from sensor we have interfaced directly with receiver chip before going with SerDes solution. REFCLK on the deserialiser was chosen 24MHz 1.8V free-running oscillator with filtered supply and 33Ω serial resistor on clock line. On the receiver side there is also single MIPI lane to receiver chip. Coax is AC coupled with 100nF 0201 chip capacitors (size constraint, again)
There are some issues. While I can configure remote I²C slaves without any issues (confirmed with logic analyzer) I do have framedrops due to receiver losing lock. I can provide Altium project for review and also provide measurements, however now limited due to test hardware failures.