Part Number: DS90UB934-Q1
Other Parts Discussed in Thread: ALP
Tool/software: TI C/C++ Compiler
We use isx 019 + 933 to connect 964, and we can receive data normally. However, if we use isx 019 + 933 to connect with 934, we cannot receive data. The lock pin is high, but 934 has no data output. Imx225 + 933 connects 934 and 964, and both can receive data. All cameras use an external clock. The 934 register refers to the configuration of 964.
934 register config:
0x01,0x01 0x4c,0x02 0x58,0x58 0x6d,0x7f 0x6e,0xaa 0x11,0x91 0x1a,0x4c 0x1b,0x0b 0x1c,0x07 0x18,0x01
And the register 0x58,0x5c,0x5d,0x65,0x6e of 934 is failed to set.How do i solve this?
What's the difference between 934 and 964 for the 933 + ISX 019?