This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640: The electrical characteristic of TD/RD/SD

Part Number: DP83640

Hi Team,

  

      The customer wants to know the electric characteristic of  pin TD/RD/SD.

      These seems not be specified in the datasheet.

       Would you kindly help to provide?

Thanks

Sincerely,

Edward

  • Hi Team,

          Sorry for bothering. Do we have information like Vin cm, Vin diff and other electric characteristic spec regarding these input pins?

          Would you kindly advise?

    Sincerely,

    Edward

  • Hi Edward,

    Pin TD/RD are the ethernet pins and have electrical specs as per 100BT and 10BT IEEE standard.There is no spec for Vin cm, Vin diff for these pins.

    Pin SD is the single ended cmos output and that also does not have Vin cm, Vin diff specs. For other specs (VIOH/VOL etc) do refer to datasheet for the IO specs.

    Let us know if there is a specific usecase that customer is looking for these pins and we can review the pin's characteristic based on the application

    --

    Regards,

    Vikram

  • Hi Vikram,

        Thanks for your feedback.

         The customer is using DP83640 in 100Base-FX fiber interface. 

          Is the spec of 100BT and 10BT IEEE standard also suitable for 100Base-FX?

          If we don't have the spec for these pins in DP83640, could we reference to our other phy?

    Thanks

    Sincerely,

    Edward

     

  • Hi Vikram,

     

         Would you kindly advise?

    Sincerely,

    Edward

  • Hello Edward,

    Yes for 100Base-Fx also there is a standard spec document : ANSI X3.263-1995 and we are compliant with the standard.

    With any standard compliant fiber transreciever and application circuit (as shown in datasheet), customer will not face any issue.

    --

    Regards,

    Vikram