Part Number: DS90UB947-Q1
Hi team,
customer's display only have 1channel LVDS input, the resolution is 1920*720, clock of LVDS is 85MHz(typ) ~104MHz(max)
they would like to use 947&948 in this project,and have below solution:
1. CPU output 1-lane LVDS to 947 /948, then output 1channel LVDS to display
2. CPU outptu 2-lane LVDC to 947/948, then output 1channle LVDS to display
the questions as below:
(1) which solution is recommended in this case? Can 947/948 be used in solution 2?
(2) For solution 1, since the clock 85MHz(type) is in the range of 947/948 CLK, but the max is not. we have concern about this
(3) The register of 0x49 FPD_TX_MODE can set the outptu mode.Can we use this register to set the signle output or Dual?
(4) Generally, what distance can be transmitted through FPD line?
thanks.