Part Number: DP83848K
Dear TI Team
I have a question about land patterns and solder paste examples.
As shown in the above figure, the data sheet p.78 states that the through-hole diameter is Φ0.2 mm,
but from our customers, the through-hole diameter is Φ0.3 mm and the dimensions of the red circle in the left figure are □ 1.18 mm. I have received a request to design at.
Is there anything wrong with the above design?
Best Regards,
Y.Ottey