Part Number: TPS65988
Other Parts Discussed in Thread: TPS25750
Hello,
I have a FTDI USB-to-I2C device connected to the TPS65988.
I am able to communicate with the device using the Application Customization software provided by TI.
There is a test option where I can read the SPI Flash over I2C and see the first few bytes.
However, I am unable to find the option where I can program the SPI Flash over I2C.
The option to program the SPI Flash hints that I should be using an USB-to-SPI adapter to program the SPI Flash.
There is an application note with example software which shows how to program the SPI Flash over I2C so I know it is possible.
Does the functionality to program the SPI Flash over I2C exist in the Application Customization Tool or will I need to develop my own software to do that?
Thanks.