Part Number: DS90UB954-Q1
Hi
We use TI DS90UB954+953 for an extended camera solution.
We would like to use synchronous mode for the design. So we will connect a crystal on 954.
From the specification of 954, typically REFCLK connected to 23- to 26-MHz reference oscillator.
Is this means the image sensor on the 953 side should be 23 to 26MHz?
Now we use Sony IMX307 + 953. The reference clock of IMX307 must to be 37.125MHz.
Not sure if the 954+953 can support IMX307 or not?