This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: DS90UB948-Q1 and DS15BR401

Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: DS15BR401

Hello. I have a board with a repeater based on the DS90UB948 and DS90UB947 chips and DS15BR401 buffers. The board should display images on 2 displays and connect to the next board in repeater mode.
Display G286HAN01.0 has 2 lvds interface. Inside it, each LVDS pair is terminated with a 50 ohm resistor. (not 100 ohms).


I'm using DS15BR401 buffers, which have 100 ohm resistors inside the output. When the display is connected, the total resistance becomes 33 ohms.


The display shows information well, but I doubt the correctness of the termination of the lvds line. On the oscillogram, the lvds signals at the output of the buffers change as if by a wave. And the signal at the input of the buffers is clean. Maybe I incorrectly terminated lvds or selected buffers?