Part Number: TVS1400
Other Parts Discussed in Thread: TVS0500, TVS0701,
Hi,
In my earlier post i had raised the below query
Planning to use TVS1400 on 12V DC line and TVS0500 on 6.2V DC Line. Since on TVS0500 VRWM is 5V, but the Clamping voltage is 9.2V and the Vbr is around 7.7V Are my part selection OK
and the response was
TVS0500 will not work as intended on a 6.2V DC line. We recommend that the DC voltage should be either equal or less than the working voltage to avoid any conduction, unnecessary clamping or leakage. You will have to step up the device used to TVS1400.
I have gone through the datasheet once again, though the Vrwm is 5V, but the actual clamping and the breakdown for this device is more than 7V. So please let me know why we cannot use this device for 6.2V Rail.
I have attached TVS0500 for your reference. From the FIg1, Fig2, Fig5,(on Page 7) it looks like the device can be used until 7V. Please provide your feedback
Regards,
Sudarshan