This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: Program SPI flash by using external programmer

Part Number: TUSB9261

Hi 

I've tried to program the 1.06 firmware bin file by using SPI flash programmer like www.dediprog.com/product/SF100  or www.sofi-tech.com/English/Product/2837405012.html

After that, I reworked the Flash part back to the PCB board then powered on, Linux always show below message when performing lsusb command

Bus 002 Device 004: ID 0451:926b Texas Instruments, Inc. TUSB9260 Boot Loader
Bus 002 Device 003: ID 0451:926b Texas Instruments, Inc. TUSB9260 Boot Loader

It looks like the FW can not be loaded correctly through this method. Do TUSB9261's FW have to be programmed on-line by TI's burner tool?

If so, I have concern about this ,because the Flash part is usually pre-programmed then SMD to the PCB in mass production for saving the working hours.