Part Number: DS280DF810
Hello,
Thank you very much for your kindly reply. I have a few other questions as below.
1. The retimer does not terminate the FEC even the CDR disabled?
2. if the CDR is disabled, how much output jitter will increase?
3. Could you please to help confirming the serdes rate and design as the attachment can be supported? (26.5625Gbps\25.78125Gbps\10.3125Gbps\1.25Gbps)
4. For the connection with switch, data should be send to two switch at same time and select one of them to receive. Does it support?
5. what is the max propagation delay?
Thanks a lot!5633.Design with DS280DF810.docx