Part Number: TUSB564RNQEVM
Other Parts Discussed in Thread: TUSB564
Hi Team,
I'm trying to evaluate TUSB564RNQEVM.
I looked at the "Doesn't Work in Specific Flip Configuration" forum.
So I checked to see if FLIP would work without using J1 (J1 is open).
Even if I don't use J1, FLIP doesn't work.
When type-C cable is connected by up-side, no image is displayed on the display monitor.
if type-C cable is connected by down-side, the image is output.
The following are the results of checking J1(2pin) voltage.
> type-C cable up-side ----- J1(2pin) voltage is 0V.
> type-C cable down-side ---- J1(2pin) voltage is 3.3V.
I have confirmed that type-C orientation is handled automatically.
But, No image output to the monitor when Type C is up-side.
Please tell me what I'm doing wrong.
or is TUSB564RNQEVM broken?
best regards.
Hitotsuyama