Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
I'm checking that this design is valid, and if so, would like to check that the 83869 is configured properly:
SWITCH MAC <= SGMII => DP83869 <= RGMII => Sitara CPSW eMAC1
I have the 83869 configured in RGMII=> SGMII Bridge mode. Register 0x01DF contains 0x0043 derived from strap configuration. register 0x6e contains 0x0600. I get no link
Register 0x05 contains 0x0000. register 0x0a also contains all 0's. for autonegotiation, which interface is the autonegotiation happening on in bridge mode?
Could someone also clarify the function and definition of bits 10,11,12 in GEN_CFG1Register(Address= 0x9)? specifically when in the bridge mode.
Regarding the document "Understanding different modes of operation in DP83869"(SNLA318), there seems to be some confusing typos. specifically, in section 1.5 "SGMII-to-RGMIIB ridge", there are instances where it refers to "RGMII-to-SGMII", i believe this is an error.
Also, in SNLA318, It refers to the SGMII interface as the "Serdes" interface. does this mean that 1000BASE-X “auto-negotiation” is used, or do the same MAC&PHY auto-negotiation rules apply?