Part Number: SN65DSI86
Hello expert,
May we know if SN65DSI86 could support 1920x1080 resolution with single channel application? Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ann Lien
Assume pixel clock = 148.5MHz, with 24BPP, we would have
Stream bit rate = 148.5 * 24 = 3.564Gbps
Min DSI Clock = Stream bit rate / (2 * DSI lane)
Max DSI clock frequency is 750MHz. So you would need 4 DSI lanes to not violate the 750MHz requirement.
Thanks
David