Part Number: TPS65988
Hi,
I am working on TPS65988 based design.
I need to know whether the GPIOs in TPS65988 has an input level of 1.8V alone or can it accepts 3.3V GPIO input level also?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65988
Hi,
I am working on TPS65988 based design.
I need to know whether the GPIOs in TPS65988 has an input level of 1.8V alone or can it accepts 3.3V GPIO input level also?
Hello,
I've assigned this issue to the relevant expert who will get back to you shortly
Hello,
The absolute maximum rating for the GPIO pins is 3.6 V, as shown in Table 6.1 of the datasheet. The recommended maximum GPIO voltage is to the LDO_3V3 rail. In addition, the high level input voltage GPIO_VH has a minimum of 1.8 V. I see no problem using 3.3 V for the GPIOs.
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.