Part Number: TPS25750
Hello,
According to datasheet, I believe that PPHV can be used as "Source" (I refered to "Figure 10-2. Power Source and Sink configuration with the Battery Charger (BQ)" of "10.1.1 USB-PD Power Application Design Considerations".)
However, Absolute max and "Ipp_hv" define only "sink current".
(Ipp_hv is defined "VBUS_IN to PPHV". I understood this means "Sink" mode.)
Q1. Is my understanding that "PPHV" can be used as "Source" correct ? (Since "VBUS_IN" is defined as only "input" at "TPS25750D Pin Functions", I asked.)
Q2. If answer of Q1 is yes, could you please tell me source current capability ?
BR,