Other Parts Discussed in Thread: TUSB2077A, TPS2042
Hi,
We are using TUSB2077A hub in freescaele iMX27 based system with windows CE 6.0.
In our design USB host1 of the processor is connected to TUSB1105RGTR which in turn is expanded through the hub TUSB2077A hub.
We are facing a problem with USB device connected to this. When we connect a BUS powered device it gets detected during boot up and works fine. But if we connect a self powered device it is not getting detected in the bootup. We have to disconnect and reconnect the device in order for it to get detected.
Kindly help us in fixing this issue.