This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E-EVM: Cannot get link to establish with DP83822 portion of DP83TD510E-EVM

Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO, MSP-EXP430G2ET, MSP430F5529, DP83TD510E

So, I have two of the DP83TD510E-EVM kits and both are powered using the USB cable interface (shorted J9).  I have them connected to a couple of Raspberry Pi single board computers via a switch/hub.  I can't get these modules to establish a link with the RPi or the switch.  When I use 100BASE-T1 cards I have to force one to be MASTER and the other to be SLAVE.  Do I need to do something to the EVM modules to get them to link up like I do with the 100BASE-T1 modules operating over the same cable/switch/RPi combo?

  • Hi Wayne,

    Please ensure that LED_0 is strapped low, J20 should be set to '0' position. This will ensure the DP83TD510 is configured in RMII Master mode, supplying the 50MHz clock to the DP83822 in RMII Slave mode. 

    The DP83822 requires the XI clock to be present at power-up or reset. So if the DP83822 is not connected to the DP83TD510 board at power-up, a reset is needed on the DP83822 after XI is present. 

    Finally, in order to establish a link between the DP83TD510 devices, an initialization script needs to be run to for our sample-able silicon available now. You can use the scripts below to establish a link through auto-negotiation or forcing the Master/Slave configuration using the USB-2-MDIO tool.

    Please note, that when using the Forced Mode scripts, extended register access should be set to "NO" in the USB-2-MDIO tool. 

    begin
    001f 8000 //hard reset
    0608 003b //disable_0_transition
    0862 39f8 //AGC Gain during Autoneg
    081a 67c0 //deq offset for 1V swing
    081c fb62 //deq offset for 2.4V swing
    0830 05a3 //Enable energy lost fallback
    0855 1b55 //MSE Threshold change
    0831 0403 //energy detect threshold
    0856 1800 //good1 MSE threshold change
    0857 8fa0 //Enable fallback to phase 1 on watchdog trigger
    0871 000c //TED input changed to slicer_in without FFE
    0883 022e //Enable Rx Filter, Change PGA threshold for Short Cable detection
    0402 1800 //Adjusr LD swing
    0878 2248 //Change PI up/down polarity
    010c 0008 //tx filter coefficient
    0112 1212 //tx filter scaling factor
    0809 5c80 //AGC retrain
    0803 1529 //Master Ph1 Back-off
    0804 1a33 //Master Ph1 Back-off
    0805 1f3d //Master Ph1 Back-off
    0850 045b //hybrid gain & delay
    0874 6967 //kp step 0 for master
    0852 7800 //FAGC init gain
    0806 1e1e //Master/Slave Ph2 Back-off
    0807 2525 //Master/Slave Ph2 Back-off
    0808 2c2c //Master/Slave Ph2 Back-off
    0850 0590 //Hybrid Gain/Delay Code
    0827 4000 //Echo Fixed Delay
    0849 0fe4 //Hybrid Cal enable
    084b 04b5 //Echo Score Sel
    001f 4000 //soft reset
    end

    begin
    001f 8000 //hard reset
    000d 0007 
    000e 0200
    000d 4007
    000e 0000 //disable auto-neg through extended register MMD 07
    000d 0001 
    000e 0834
    000d 4001
    000e 4000 //force master mode through extended register MMD 01
    000d 0001 
    000e 08f6
    000d 4001
    000e 0000 //force 1.0v swing through extended register MMD 01
    000d 001F 
    000e 0608 
    000d 401F 
    000e 003b //disable_0_transition
    000d 001F 
    000e 0862 
    000d 401F 
    000e 39f8 //AGC Gain during Autoneg
    000d 001F 
    000e 081a 
    000d 401F 
    000e 67c0 //deq offset for 1V swing
    000d 001F 
    000e 081c 
    000d 401F 
    000e fb62 //deq offset for 2.4V swing
    000d 001F 
    000e 0830 
    000d 401F 
    000e 05a3 //Enable energy lost fallback
    000d 001F 
    000e 0855 
    000d 401F 
    000e 1b55 //MSE Threshold change
    000d 001F 
    000e 0831 
    000d 401F 
    000e 0403 //energy detect threshold
    000d 001F 
    000e 0856 
    000d 401F 
    000e 1800 //good1 MSE threshold change
    000d 001F 
    000e 0857 
    000d 401F 
    000e 8fa0 //Enable fallback to phase 1 on watchdog trigger
    000d 001F 
    000e 0871 
    000d 401F 
    000e 000c //TED input changed to slicer_in without FFE
    000d 001F 
    000e 0883 
    000d 401F 
    000e 022e //Enable Rx Filter, Change PGA threshold for Short Cable detection
    000d 001F 
    000e 0402 
    000d 401F 
    000e 1800 //Adjusr LD swing
    000d 001F 
    000e 0878 
    000d 401F 
    000e 2248 //Change PI up/down polarity
    000d 001F 
    000e 010c 
    000d 401F 
    000e 0008 //tx filter coefficient
    000d 001F 
    000e 0112 
    000d 401F 
    000e 1212 //tx filter scaling factor
    000d 001F 
    000e 0809 
    000d 401F 
    000e 5c80 //AGC retrain
    000d 001F 
    000e 0803 
    000d 401F 
    000e 1529 //Master Ph1 Back-off
    000d 001F 
    000e 0804 
    000d 401F 
    000e 1a33 //Master Ph1 Back-off
    000d 001F 
    000e 0805 
    000d 401F 
    000e 1f3d //Master Ph1 Back-off
    000d 001F 
    000e 0850 
    000d 401F 
    000e 045b //hybrid gain & delay
    000d 001F 
    000e 0874 
    000d 401F 
    000e 6967 //kp step 0 for master
    000d 001F 
    000e 0852 
    000d 401F 
    000e 7800 //FAGC init gain
    000d 001F 
    000e 0806 
    000d 401F 
    000e 1e1e //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0807 
    000d 401F 
    000e 2525 //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0808 
    000d 401F 
    000e 2c2c //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0850 
    000d 401F 
    000e 0590 //Hybrid Gain/Delay Code
    000d 001F 
    000e 0827 
    000d 401F 
    000e 4000 //Echo Fixed Delay
    000d 001F 
    000e 0849 
    000d 401F 
    000e 0fe4 //Hybrid Cal enable
    000d 001F 
    000e 084b 
    000d 401F 
    000e 04b5 //Echo Score Sel
    000d 001F 
    000e 0018 
    000d 401F 
    000e 0043 //Set CRS/RX_DV pin as RX_DV for RMII repeater mode
    000d 001F 
    000e 001f 
    000d 401F 
    000e 4000 //soft reset
    end

    begin
    001f 8000 //hard reset
    000d 0007 
    000e 0200
    000d 4007
    000e 0000 //disable auto-neg through extended register MMD 07
    000d 0001 
    000e 0834
    000d 4001
    000e 0000 //force slave mode through extended register MMD 01
    000d 0001 
    000e 08f6
    000d 4001
    000e 0000 //force 1.0v swing through extended register MMD 01
    000d 001F 
    000e 0608 
    000d 401F 
    000e 003b //disable_0_transition
    000d 001F 
    000e 0862 
    000d 401F 
    000e 39f8 //AGC Gain during Autoneg
    000d 001F 
    000e 081a 
    000d 401F 
    000e 67c0 //deq offset for 1V swing
    000d 001F 
    000e 081c 
    000d 401F 
    000e fb62 //deq offset for 2.4V swing
    000d 001F 
    000e 0830 
    000d 401F 
    000e 05a3 //Enable energy lost fallback
    000d 001F 
    000e 0855 
    000d 401F 
    000e 1b55 //MSE Threshold change
    000d 001F 
    000e 0831 
    000d 401F 
    000e 0403 //energy detect threshold
    000d 001F 
    000e 0856 
    000d 401F 
    000e 1800 //good1 MSE threshold change
    000d 001F 
    000e 0857 
    000d 401F 
    000e 8fa0 //Enable fallback to phase 1 on watchdog trigger
    000d 001F 
    000e 0871 
    000d 401F 
    000e 000c //TED input changed to slicer_in without FFE
    000d 001F 
    000e 0883 
    000d 401F 
    000e 022e //Enable Rx Filter, Change PGA threshold for Short Cable detection
    000d 001F 
    000e 0402 
    000d 401F 
    000e 1800 //Adjusr LD swing
    000d 001F 
    000e 0878 
    000d 401F 
    000e 2248 //Change PI up/down polarity
    000d 001F 
    000e 010c 
    000d 401F 
    000e 0008 //tx filter coefficient
    000d 001F 
    000e 0112 
    000d 401F 
    000e 1212 //tx filter scaling factor
    000d 001F 
    000e 0809 
    000d 401F 
    000e 5c80 //AGC retrain
    000d 001F 
    000e 0803 
    000d 401F 
    000e 1529 //Master Ph1 Back-off
    000d 001F 
    000e 0804 
    000d 401F 
    000e 1a33 //Master Ph1 Back-off
    000d 001F 
    000e 0805 
    000d 401F 
    000e 1f3d //Master Ph1 Back-off
    000d 001F 
    000e 0850 
    000d 401F 
    000e 045b //hybrid gain & delay
    000d 001F 
    000e 0874 
    000d 401F 
    000e 6967 //kp step 0 for master
    000d 001F 
    000e 0852 
    000d 401F 
    000e 7800 //FAGC init gain
    000d 001F 
    000e 0806 
    000d 401F 
    000e 1e1e //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0807 
    000d 401F 
    000e 2525 //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0808 
    000d 401F 
    000e 2c2c //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0850 
    000d 401F 
    000e 0590 //Hybrid Gain/Delay Code
    000d 001F 
    000e 0827 
    000d 401F 
    000e 4000 //Echo Fixed Delay
    000d 001F 
    000e 0849 
    000d 401F 
    000e 0fe4 //Hybrid Cal enable
    000d 001F 
    000e 084b 
    000d 401F 
    000e 04b5 //Echo Score Sel
    000d 001F 
    000e 0018 
    000d 401F 
    000e 0043 //Set CRS/RX_DV pin as RX_DV for RMII repeater mode
    000d 001F 
    000e 001f 
    000d 401F 
    000e 4000 //soft reset
    end

    begin
    
    000d 001F 
    000e 001f 
    000d 401f 
    000e 8000 //hard reset
    000d 0007 
    000e 0200 
    000d 4007 
    000e 0000 //disable autoneg MMD 07
    000d 0001 
    000e 0834 
    000d 4001 
    000e 4000 //Force Master Mode MMD 01
    000d 0001 
    000e 08f6 
    000d 4001 
    000e 1000 //Force 2.4V swing MMD 01
    000d 001F 
    000e 0608 
    000d 401f 
    000e 003b //disable_0_transition
    000d 001F 
    000e 0862 
    000d 401f 
    000e 39f8 //AGC Gain during Autoneg
    000d 001F 
    000e 081a 
    000d 401f 
    000e 67c0 //deq offset for 1V swing
    000d 001F 
    000e 081c 
    000d 401f 
    000e fb62 //deq offset for 2.4V swing
    000d 001F 
    000e 0830 
    000d 401f 
    000e 05a3 //Enable energy lost fallback
    000d 001F 
    000e 0855 
    000d 401f 
    000e 1b55 //MSE Threshold change
    000d 001F 
    000e 0831 
    000d 401f 
    000e 0403 //energy detect threshold
    000d 001F 
    000e 0856 
    000d 401f 
    000e 1800 //good1 MSE threshold change
    000d 001F 
    000e 0857 
    000d 401f 
    000e 8fa0 //Enable fallback to phase 1 on watchdog trigger
    000d 001F 
    000e 0871 
    000d 401f 
    000e 000c //TED input changed to slicer_in without FFE
    000d 001F 
    000e 0883 
    000d 401f 
    000e 022e //Enable Rx Filter, Change PGA threshold for Short Cable detection
    000d 001F 
    000e 0402 
    000d 401f 
    000e 1800 //Adjusr LD swing
    000d 001F 
    000e 0878 
    000d 401f 
    000e 2248 //Change PI up/down polarity
    000d 001F 
    000e 010c 
    000d 401f 
    000e 0008 //tx filter coefficient
    000d 001F 
    000e 0112 
    000d 401f 
    000e 1212 //tx filter scaling factor
    000d 001F 
    000e 0809 
    000d 401f 
    000e 5c80 //AGC retrain
    000d 001F 
    000e 0803 
    000d 401f 
    000e 1529 //Master Ph1 Back-off
    000d 001F 
    000e 0804 
    000d 401f 
    000e 1a33 //Master Ph1 Back-off
    000d 001F 
    000e 0805 
    000d 401f 
    000e 1f3d //Master Ph1 Back-off
    000d 001F 
    000e 0850 
    000d 401f 
    000e 045b //hybrid gain & delay
    000d 001F 
    000e 0874 
    000d 401f 
    000e 6967 //kp step 0 for master
    000d 001F 
    000e 0852 
    000d 401f 
    000e 7800 //FAGC init gain
    000d 001F 
    000e 0806 
    000d 401f 
    000e 1e1e //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0807 
    000d 401f 
    000e 2525 //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0808 
    000d 401f 
    000e 2c2c //Master/Slave Ph2 Back-off
    000d 001F 
    000e 0850 
    000d 401f 
    000e 0590 //Hybrid Gain/Delay Code
    000d 001F 
    000e 0827 
    000d 401f 
    000e 4000 //Echo Fixed Delay
    000d 001F 
    000e 0849 
    000d 401f 
    000e 0fe4 //Hybrid Cal enable
    000d 001F 
    000e 084b 
    000d 401f 
    000e 04b5 //Echo Score Sel
    000d 001F 
    000e 001f 
    000d 401f 
    000e 4000 //soft reset
    
    end

    begin
    
    000d 001f 
    000e 001f 
    000d 401f 
    000e 0000 //hard reset
    000d 0007 
    000e 0200 
    000d 4007 
    000e 0000 //disable autoneg MMD 07
    000d 0001 
    000e 0834 
    000d 4001 
    000e 0000 //Force Slave Mode MMD 01
    000d 0001 
    000e 08f6 
    000d 4001 
    000e 1000 //Force 2.4V swing MMD 01
    000d 001f 
    000e 0608 
    000d 401f 
    000e 003b //disable_0_transition
    000d 001f 
    000e 0862 
    000d 401f 
    000e 39f8 //AGC Gain during Autoneg
    000d 001f 
    000e 081a 
    000d 401f 
    000e 67c0 //deq offset for 1V swing
    000d 001f 
    000e 081c 
    000d 401f 
    000e fb62 //deq offset for 2.4V swing
    000d 001f 
    000e 0830 
    000d 401f 
    000e 05a3 //Enable energy lost fallback
    000d 001f 
    000e 0855 
    000d 401f 
    000e 1b55 //MSE Threshold change
    000d 001f 
    000e 0831 
    000d 401f 
    000e 0403 //energy detect threshold
    000d 001f 
    000e 0856 
    000d 401f 
    000e 1800 //good1 MSE threshold change
    000d 001f 
    000e 0857 
    000d 401f 
    000e 8fa0 //Enable fallback to phase 1 on watchdog trigger
    000d 001f 
    000e 0871 
    000d 401f 
    000e 000c //TED input changed to slicer_in without FFE
    000d 001f 
    000e 0883 
    000d 401f 
    000e 022e //Enable Rx Filter, Change PGA threshold for Short Cable detection
    000d 001f 
    000e 0402 
    000d 401f 
    000e 1800 //Adjusr LD swing
    000d 001f 
    000e 0878 
    000d 401f 
    000e 2248 //Change PI up/down polarity
    000d 001f 
    000e 010c 
    000d 401f 
    000e 0008 //tx filter coefficient
    000d 001f 
    000e 0112 
    000d 401f 
    000e 1212 //tx filter scaling factor
    000d 001f 
    000e 0809 
    000d 401f 
    000e 5c80 //AGC retrain
    000d 001f 
    000e 0803 
    000d 401f 
    000e 1529 //Master Ph1 Back-off
    000d 001f 
    000e 0804 
    000d 401f 
    000e 1a33 //Master Ph1 Back-off
    000d 001f 
    000e 0805 
    000d 401f 
    000e 1f3d //Master Ph1 Back-off
    000d 001f 
    000e 0850 
    000d 401f 
    000e 045b //hybrid gain & delay
    000d 001f 
    000e 0874 
    000d 401f 
    000e 6967 //kp step 0 for master
    000d 001f 
    000e 0852 
    000d 401f 
    000e 7800 //FAGC init gain
    000d 001f 
    000e 0806 
    000d 401f 
    000e 1e1e //Master/Slave Ph2 Back-off
    000d 001f 
    000e 0807 
    000d 401f 
    000e 2525 //Master/Slave Ph2 Back-off
    000d 001f 
    000e 0808 
    000d 401f 
    000e 2c2c //Master/Slave Ph2 Back-off
    000d 001f 
    000e 0850 
    000d 401f 
    000e 0590 //Hybrid Gain/Delay Code
    000d 001f 
    000e 0827 
    000d 401f 
    000e 4000 //Echo Fixed Delay
    000d 001f 
    000e 0849 
    000d 401f 
    000e 0fe4 //Hybrid Cal enable
    000d 001f 
    000e 084b 
    000d 401f 
    000e 04b5 //Echo Score Sel
    000d 001f 
    000e 001f 
    000d 401f 
    000e 4000 //soft reset
    
    end

    .

    Regards,

    Justin 

  • Thanks Justin,

    The setting for J20 helped to light up the link light between the computer and the RJ45 but the two DP83TD510E-EVM kits won't establish or promote a link that I can drive traffic through.  I haven't implemented your scripts because I'm still having trouble connecting to the boards using the USB-2-MDIO tool.  The DP83TD510E-EVM board combination is the only thing connected to my PC via a USB cable. 

    Looking at the guide for the USB-2-MDIO it says that I need the MSP430F5529 USB LaunchPad Evaluation Kit.  So if that's true, I have two on order for Monday arrival as well as two of the MSP-EXP430G2ET.  If the LaunchPad Evaluation Kit is not needed, are there any tips for connecting the PC and USB-2-MDIO program to the board?  I am powering the board with the same USB cable I'm trying to connect with.  The USB power jumper (J9) is shorted.  The other 10 jumpers are in the state they arrived in which means nothing is connected to any of the four posts making up J3 and J20 was changed per your suggestion (photo passed in below).

    Sincerely,

    Wayne

  • Hi Wayne,

    Can you confirm that you see the same results if you power the DP83TD510 EVM through the 5V supply on J12?

    Regards,
    Justin 

  • Hi Justin,

    The powering of the device with a proper power supply changed things.  It responds to the USB-2-MDIO now.  I removed the USB power jumper.

    So in this mode I'll run the AutoNegotiation_Initialization.txt and Force_1Vpp_Master_Init on one of the board combos and the AutoNeg and Slave script on the other board combo (in that order)?

    Making progress!  This is good news!

    -Wayne

  • Hi Wayne,

    There are three possible configurations to run to establish a link between the DP83TD510E boards:

    1. AutoNegotiation_Initialization.txt on both Board A and Board B. (Extended registers menu should be set to "YES")

    2. Force_1Vpp_Master_Init.txt on Board A and Force_1Vpp_Slave_Init.txt on Board B. (Extended registers menu should be set to "NO")

    3. Force_2p4Vpp_Master_Init.txt on Board A and Force_2p4Vpp_Slave_Init.txt on Board B. (Extended registers menu should be set to "NO")

    Please do not run both Auto-Negotiation and Forced mode script on the same board. 

    Regards,
    Justin