Part Number: SN65HVD74
Other Parts Discussed in Thread: ISO1410,
Hi everyone,
I am trying to use the SN65HVD74D full-duplex RS-485 transceiver to connect the full-duplex transceiver to a half duplex device. This is because we are short on the half-duplex transceivers ISO1410 and currently in need to do this as soon as possible.
Hence I would like to know if it is possible. Is there a way to do this? Can someone suggest?
Thanks in advance,
-Chandrasekhar DVS