Part Number: DS90UB914A-Q1
Hi,
Because the AP only have 8bit digital port
So I want to know if DS90UB914A can use ROUT[7:0] to output data to AP?
if so,which register of DS90UB914A is use to config the output pin?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB914A-Q1
Hi,
Because the AP only have 8bit digital port
So I want to know if DS90UB914A can use ROUT[7:0] to output data to AP?
if so,which register of DS90UB914A is use to config the output pin?
Thanks
Hello Wang,
There is no special configuration needed for this in SW. Just make sure that the partner serializer device like 913A is using data inputs DIN0-7, and those will be passed through to ROUT0-7 on 914A automatically
Best Regards,
Casey