Part Number: DS64BR111
Hello,
We have approximately 20 inches of copper length on PCB (FR4) between outputs of ds64br111 to receiver (with 2 contacts on the way). The receiver has equalization on input (set to equalize 18 inch over FR4).
Can you suggest a sufficient level of de-emphasis on the output of ds64br111?
The receiver can handle 0,4Vdiffp-p to 2.0diffp-p max on input so the default VOD on output seems to be enough (700mV on channel A and 1000mV on channel B).
Br Mikael