Part Number: TUSB8042
I want to use this part to expand one USB3.1 port from the CPU to 4 ports.
I can't be sure, but it looks like I don't need to connect I2C or an external EEPROM.
I want to be able to control the current limit on 3 of the ports and don't want to have to program the part.
Can the part be used with default settings without programming?
W. Tustin