Part Number: MAX3221E
When I Send data from the mcu , Connect the MAX3221E Pin8 and Pin13 , the data is correct ,
When connect the board to PC , the RS232 TX is incorrect , likely clock inferrence
the wave as below :
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3221E
When I Send data from the mcu , Connect the MAX3221E Pin8 and Pin13 , the data is correct ,
When connect the board to PC , the RS232 TX is incorrect , likely clock inferrence
the wave as below :
Hi,
Is this the data from MCU to MAX3221E? Can you compare the waveform with and without loop back? Similarly can you check the bus signal level with and without loop back? RS232 signal should be around -5V to 5V. What's data rate of the application?
Regards,
Hao