Part Number: TUSB522P
Hi, I am going to use TUSB522p for my USB System.
I have a simple question.
In the datasheet, in the typical application like below,
OS1 and OS2 Pins are both Pull-Up, and Pull-down with 47k Ohm.
I understand that EQ, and DE pins have Mid level input, but OS1 and OS2 Pins only have High or Low Cmos input.
If I put both pull up and pull down like typical application then what logic value will OS1 and OS2 will have?
Thanks.