Part Number: DS15BR400
We are using DS15BR400TSQ in our new project and we are having some issues. While input signal looks perfectly OK, the output , however, looks like modulated input. Pre-emphasis was turned off in this measurement. We triple-checked everything (Schematics, Soldered components, Layout) but can't really find anything that would be causing this modulation. Could you provide any explanation for this modulation? Output is connected to terminated FPGA LVDS input. We have an older version of the board without DS15BR400TSQ where FPGA output drives FPGA input directly - no issues here. The new PCB version has DS15BR400TSQ inserted in between FPGA output and input. Connection between inputs and outputs is made using RJ45 connectors and 50cm STP cable (On both PCB versions). The idea behind using DS15BR400TSQ was to extend communication range (FPGA inputs and outputs are located on the same FPGA).