Hi
Our setup is Sensor -> 913A -> 954 -> i.MX6.
The sensor output is 12-bit parallel and the 913A/954 is configured in RAW12 mode.
The frame size is 1280x720 45fps. Pixel clock is 60MHz
The 954 is reporting a frame size of 2406 x 723.
I have scoped the input to the 913A and it matches the sensor configuration. What could be causing the frame size to be incorrect in the 954?
Thanks.