Part Number: DS25BR204
- How does the “PWDNn” Signal work? Does this signal tri-state the individual LVDS output buffer? Its not clear to me in the datasheet what is the voltage on the output of the buffers when PWDNn is asserted.
- Both the output and input are terminated with a 100Ω resistor internally. However, in the user guide schematics, the input is terminated again. Is this an indication that I need a an external 100 ohm termination as the user guide shows?