This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25810: TPS25810 IN1&IN2 and AUX application question.

Part Number: TPS25810

Hi Team,

could you please comment on the questions shown as below:

1. Does the AUX can connect on the 3.3V power rail or only can connect to 5V?

2. Could you help double check if TPS25810 can disable OUTPUT power when there isn’t device attach even power on IN1&IN2&AUX?

3. Because this device have integrated a MOSFET on VBUS, so does this means the chip itself can control the output of VBUS? There is no need to close IN1 and IN2 to achieve energy saving management.

4. If AUX supplies power to CC1 and CC2, what is the current of the entire AUX?

 B.R.

 Zhizhao