Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Hi,
For this docking project using TPS65987DDH, GPIO1 is configured as below.
This GPIO is connected from TPS65987 to a MCU GPIO directly without external pull. The default level is high as seen from above setting, and we tried to send GPsl/GPsh to change the output level.
But, when we send GPsl to drive it low but found it failed. It can work for either condition as below.
- Add a 1Mohm resistor pull-down resistor on board.
- Probe this signal from a scope (P6139B/Tektronix, 10Mohm, 8pF).
It seems a pull-down resistor on board is helpful, but we can't change the HW design now. We tried to disable "Internal pull up enable" setting but not help. Please support to provide your input.
Thanks!
Antony