Part Number: TUSB8042A
Other Parts Discussed in Thread: TUSB8041A,
Holle,
We found a issue with the TUSB8042AI.
The same device did not see this problem on TUSB8041A downstream port.
Linux xHCI driver shows the following messages:
[ 6.922975] usb 1-1.2: new full-speed USB device number 4 using xhci_hcd
[ 7.027826] usb 1-1.2: New USB device found
[ 7.039037] usb 1-1.2: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 7.046636] usb 1-1.2: Not enough bandwidth for new device state.
[ 7.052727] usb 1-1.2: can't set config #1, error -28
Do TUSB8042AI need a special xhci driver?
Not having enough bandwidth what could be a problem?
Are there any differences between anindustrial version (TUSB8042AI) & commercial version(TUSB8041A) ?
BR.
Innis.