Part Number: SN65DSI83
Other Parts Discussed in Thread: DSI-TUNER
Dears
I want to use with the following specifications
◆ MIPI DSI
total 2200 (H) x1125 (V) (active 1920 (H) x1080 (V))
mode RGB888 = 24bit
fps 60
Therefore, the total bandwidth is 2200x1125x24x60 = 3.564Gbps.
MIPI is considering 4lane, so 891Mbps.
MIPI is 1 Gbps / lane, we believe that it will meet the required specifications.
◆ LVDS
total 2200 (H) x1125 (V)
active 1920 (H) x1080 (V)
mode RGB888 = 24bit , DE / H / V / 0 is added, 28bit.
fps 60
Therefore, the total bandwidth is 2200x1125x28x60 = 4.158Gbps.
LVDS is 1039.5Mbps per lane.
Question
Is there anything wrong with the above specifications?
Sincerely,