Part Number: TCA9554
TCA9554 datasheet shows "when an I/O in configured as an input, input voltage may be raised above VCC", what is the voltage range for the I/O when used as input? Can I/O lower than VCC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9554
TCA9554 datasheet shows "when an I/O in configured as an input, input voltage may be raised above VCC", what is the voltage range for the I/O when used as input? Can I/O lower than VCC?
Technically our I/O pins are 5V tolerant though if you use Vcc at for example 3.3V and pull the pin to 5V, you may see additional Icc current that is no longer in spec with the datasheet's electrical parameters.
Using the device at a lower voltage than Vcc will result in higher shoot through currents resulting in higher supply current readings.
If for some reason you need use your device at a different logic range than the I2C lines, you can use TCA64xx as it acts as a level translator between I2C logic and p-port logic.
-Bobby