This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: DP83867ISRGZT connection with FPGA

Part Number: DP83867IS


Hi Team,

I received the following request.

Could you, please, help?

 #############################################################################

We are connecting a Xilinx FPGA to the DP83867ISRGZT.

We have currently connected the 625MHz Clock out from SGMII_CO to a transceiver clock input on the FPGA. Our questions are related to this clock.

 

  1. Is the clock continuous? (I.e. present whether or not there is an Ethernet link present).
  2. Is the clock related to the received network clock?
  3. If so is there any change to it if the network disappears?
  4. Is there a documented jitter transfer function?

 

 #############################################################################

Regards,

Fabio