Part Number: TUSB9261
Hi There,
I have some design consideration on TUSB9261 as blew:
1. Can TUSB9261 left USB 2.0 signal as floating<Motherboard On Board Design>?any side effect or function can't work?(ex: flash firmware or compatibility issues)
etc.)
2. I want to double check the SATA trace routing impedance is 100 ohm +/-15% is correct ?
3. Is the reset goes high after power (VDD33 & VDD11) stable at least 2ms?
4. Can TUSB9261 use Winbond W25X10CLSNIG for eeprom?
5. Which firmware version can support SATA led function?
6. How can I tune the SATA signal?
7. Can the TUSB9261 setting the USB3.0 signal RX signal EQ?