Part Number: DS80PCI102
Hi Sir,
At present, the attached schematic PCI-E has no output signal, and the bypass DS80PCI102 can be pass test, but through DS80PCI102 is failure.
could help us check this schematic or suggestion.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS80PCI102
Hi Sir,
At present, the attached schematic PCI-E has no output signal, and the bypass DS80PCI102 can be pass test, but through DS80PCI102 is failure.
could help us check this schematic or suggestion.
Greetings,
I reviewed this schematic.
1). If i understand this correctly, when you use wire to bypass the device it is working fine. But when DS80PCI102 is plugged in the signal does not go through. Please confirm my understanding.
2). If #1 above is true, can you please pull RXDET pin#22 to "1" - note table 4 of the data sheet - do you see any difference?
3). To start with, please put EQA0=EQA1=EQB0=EQB1=0 or 1K to GND
4). To start with, please put VOD_SEL=DEMA=DEMB= 1K ohm to GND
Please let us know the result.
Regards,, Nasser