This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848Q-Q1: Reset Pin parmeters and behavior

Part Number: DP83848Q-Q1

Hello,

some questions about the reset pin.

1.) The DS says : The DP83848x includes an internal power-on reset (POR) function and does not need to be explicitly reset
for normal operation after power up. If required during normal operation, the device can be reset by a
hardware or software reset. --> The DS says in the pin description  I, PU. In this case it should be output as well , right ? We see that the PHY is driving the pin low.

2.) What is the value of the Pull Up on the reset Pin. I cannot find any specification.

3.)Is this specification out of the DS also valid for the Reset Pin ?

Thanks and BR Ralf