This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C189-Q1: Selection of RGB lines mapping to generate the Dual LVDS signals

Part Number: DS90C189-Q1


Hi,

We want to develop one common control card with DS90C189-Q1 Dual LVDS transceiver IC. This control card should be common to drive the various LCD panels as below. Which LCD lines mapping should be used for my application, and how to select this mapping either MSB on CH3 or LSB on CH3.

What is the meaning of MSB on CH3 and LSB on CH3.

Please let me know.

LCD part Numbers:

1. AUO make 24 Inch panel (G240HW01-V1-AUO)

2. Litemax make 24 Inch Panel (MU_DLF_DLH2425_V1)

3. Winstar make 7 Inch Panel (WF70A8SYAHLNG0)

4. Orient make 7 inch panel (AFY1024600A0)