Part Number: THVD1410
Is it acceptable to use a 1mA led on the RS485 datalines to give visual feedback about data activity?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1410
Is it acceptable to use a 1mA led on the RS485 datalines to give visual feedback about data activity?
Hi,
It's an interesting idea. Would you put the led between A and B or from A/B to ground? RS485 drives about 30mA during normal operation. If the load led creates is kind of symmetric to A and B pins, this scheme may work. However more commonly I see people put led at the receiver output (R, pin 1) as indicator.
Regards,
Hao
Thanks for your reply Hao
Input-side would also be possible, but I would prefer the LEDs to be based on the actual output.
I was thinking about putting putting the LED in between A and B. Then if a '1' is send on the dataline, the LED will blink.
Would that be possible? What would an assymetric load do, is the device protected against that in some kind of way?
edit: Or even put two leds in opposite polarity, then they will blink with any data activity.
I think the theme would work although not ideal. When '1' is sent, the voltage of A will become lower due to the extra LED load. However if the receiver input is still large enough, RS485 communication should still work.
Regards,
Hao