Other Parts Discussed in Thread: TUSB1310
Hi,
I want to know the detail of PHY_RESTEN pin function.
During RESETN pin is de-asserted and PHY_RESETN pin is asserted , is TUSB1310 outpytting PCLK & ULPI_CLK signals?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TUSB1310
Hi,
I want to know the detail of PHY_RESTEN pin function.
During RESETN pin is de-asserted and PHY_RESETN pin is asserted , is TUSB1310 outpytting PCLK & ULPI_CLK signals?
Best regards,
Thank you for your quick reply.
In the Figure of the PIPE spec "section 6.2 Reset", it is decribed that "PCLK running at any frequency less than or equal to final operational frequency".
My understanding is that "PHY continue to output the PCLK signal during Reset# is asserting".
I want to confirm that this is corret.
And I have one more question.
In the PIPE spec "section 6.1 clocking", it is described that "This clock (PCLK) may also have spread spectrum modulation."
Is the PCLK output of TUSB1310 modulated by SSC?
I'm reading the TUSB1310 Data Manual, but I don't understand it well.
Best regards,
Yes, PCLK continues to run when PIPE_RESETN is asserted low. This is done purposely so that reset logic within the DL can transition.
In a USB3 application, the PHY will normally apply SSC to its own PLL so as to modulate the output data stream. This shows up on the PIPE PCLK, as it is derived directly from the PLL clock. So, if you have SSC turned on, this will also be on the PCLK.