Part Number: TIDA-01487
Other Parts Discussed in Thread: ISO7721, SN74HC32, SN74HC04
I wish to implement the CAN isolating part of the TIDA-01487 reference design (CAN1, Bus Arbitration Logic, Isolation, CAN2), but I am using a 3.3 V architecture. From looking at the datasheets I believe the SN74HC04, AN74HC08, SN74HC32 and ISO7721 parts have recommended operating conditions which allow 3.3 V operation, however the CAN transcievers do not as they are 5 V supplied.
I have selected the SN65HVD231QD CAN transciever as a replacement for CAN1 and CAN2, which I believe will work fine - but is there something I have missed which will prevent these from working in this design? My bus will be operating as 1 Mbps.
I am also interested if there is any information on what applications this reference design has previously been applied to? My application is particularly affected by radiation and reliability requirements and as such being able to demonstrate previous design usage provides reassurance to the design.
Thanks