We have an application where we are considering the use of a serdes setup to push video across a 10 ft cable.
Can you please recommend a serdes solution for the following?
- Input: HDMI or LVDS
- Output: LVDS (4-lanes + clock)
- Resolution: 1366 x 768
- Frame rate: 30 fps
- Medium: shielded, twisted-pair (STP) cable
- Side channel: I2C
Additionally, what would be the link bandwidth for the scenario above? The video data itself is around 755 Mbps (1366 x 768 x 24 bpp x 30 fps).